Technical FAQs

Ask a Question

Can the CHOM1224L125GC be converted to a main breaker load center?

Issue:
Can we install a main breaker in a CHOM1224L125GC main lug load center?

Product Line:
Load Centers

Environment:
Canadian Homeline

Resolution:
The labeling is already on the load center, but it doesn't really state in those words that the load center can be converted to a main breaker(see attached visual of wiring diagram). The load center actually can be converted to a main breaker (QOM1) BUT they need to be careful because in Canada, even though they convert it to main breaker it cannot be used in Service Entrance. 
Was this helpful?
What can we do to improve the information ?