Technical FAQs

Ask a Question

What is the replacement blank cover and cover with numbers for part numbers TK-1811 and TK-1001?

Issue:
What are the Thermostat covers for TK-1811 and TK-1001 Stats ?

Product Line:
Field Devices

Environment:
Maintenance

Cause:
Replacement

Resolution:
The replacement cover is the AT-11-500, it is a standard cover athat comes with a blank insert.  If a standard Blank cover is needed, the part number is AT-11-404
6/22 Emailed customer reply 10:11 CDT 

 
Was this helpful?
What can we do to improve the information ?