Technical FAQs

Ask a Question

What are the dimensions of an MA-305 Actuator?

Issue:
Dimensions of MA-3xx, MA5-318, MA-4xx, and MA5-419 (Standard) Actuators.

Product Line: 
HVAC / Field Devices

Environment:
Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:​
Dimensions are in inches (mm). See diagram below


Was this helpful?
What can we do to improve the information ?