Technical FAQs

Ask a Question

What is the NEMA rating of an MA-305?

Issue:
NEMA rating for MAx-305 & MAx-318 Series MAx-405 Through MAx-419 Series actuators

Product Line: 
HVAC / Field Devices

Environment:
Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
NEMA Type 4 when used with the gasket (provided) and water-tight conduit connectors (not provided), optional hazardous location models.
Was this helpful?
What can we do to improve the information ?