Technical FAQs

Ask a Question

SQL Server log on account doesn't have permissions to write files error during ENM installation

Issue
ENM installation fails at 'Check SQL Service Permissions':

          

The error message is:
          

          SQL Server log on account doesn't have permissions to write files. Make sure the SQL service log on account can write to the database backup folder.

Product Line
Event Notification Module 8.3.3 (could apply to other versions)

Environment
Installer

Cause
SQL Server service doesn't have sufficient permission.

Resolution
Change SQL Server service permission to Local System account.
- From Windows Services open SQL Server property window
- Select Log On tab
- Select Local System account

          
 
Was this helpful?
What can we do to improve the information ?