Technical FAQs

Ask a Question

What are the rebuild kit for Vx-7xxx, Vx-8xxx and Vx-9xxx Series valves?

Product Line: 
HVAC / Field Devices

Environment:
Valves

Cause:
Replacement / Installation / Maintenance

Resolution:
See attached document for the part numbers of the rebuild kit for the Vx-7xxx / Vx-8xxx and Vx-9xxx Series valves.
Check with customer care or in BAAN for the availability of the part numbers.
Note :
Some repair kits could be obsolete even though they are listed in the document. 
Changes to availablility are subject to change without notice 
Was this helpful?
What can we do to improve the information ?