Technical FAQs

Ask a Question

What is the operating temperature of a CP-9301 actuator drive?

Issue:
Operating temperature of CP-9301 and CP-9302

Product Line: 
HVAC / Field Devices

Environment:
Actuator Drive

Cause:
Replacement / Installation / Maintenance

Resolution:
Operating temperature is -40 to 136 °F (-40 to 58 °C).
Was this helpful?
What can we do to improve the information ?