Technical FAQs

Ask a Question

What is the NEMA rating of a CP-9301 actuator drive?

Issue:
What NEMA classification rating does the CP-9301 and CP-9302 drives have?

Product Line: 
HVAC / Field Devices

Environment:
Application

Cause:
Features

Resolution:
The Drive actuators are rated NEMA Type 4; IEC IP56
Was this helpful?
What can we do to improve the information ?