Technical FAQs

Ask a Question

What is the replacement for Erie Zone valve part number 0734C0347VB40

Issue:
What is the cross for a 0734C0347VB40 zone valve with 25 PSI (7.5)CV for 1/2" valve?

Product Line:
Erie Zone Valves 

Environment:
Replacement

Cause:
Cross Reference

Resolution:
The older Erie Zone Valve had a high Cv for a small connection , 1/2".  Either a 1/2" pipe size VT2213G23B020 with a lower CV can be used , or for same CV as Erie Valve, a 3/4" VT2317G23BV020 can be used with a reducer for 3/4"-1/2" connection  .
Was this helpful?
What can we do to improve the information ?