Technical FAQs

Ask a Question

How long, how much time does it take for am VT2212 Valve to open , or close ?

Issue:
Timing of Erie VT/VS PopTop Series from full open to full close.

Product Line: 
HVAC / Field Devices

Environment:
Valves and Actuator

Cause:
Product Features 

Resolution:
Full Open to Full Close 25 Sec max for 60 Hz; 30 Sec max for 50 Hz. For Spring return, with power interruption Full Closed is 9 Sec maximum
Was this helpful?
What can we do to improve the information ?