Technical FAQs

Ask a Question

Does the HMISCU support the XVGU?

Yes, the HMISCU supports the XVGU series tower light.

It is possilbe to add the driver in Vijeo designer for the Towerlight accessory when using Somachine V4.3.

 
Was this helpful?
What can we do to improve the information ?