Technical FAQs

Ask a Question

What is the operating temperature of an MA-305?

Issue:
Operating temperature for MAx-305 & MAx-318 Series, MAx-405 Through MAx-419 Series Actuators.

Product Line: 
HVAC / Field Devices

Environment:
Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
The operating temperature of an MA-305 is -40 to 136 °F (-40 to 58 °C).
Was this helpful?
What can we do to improve the information ?