Technical FAQs

Ask a Question

Which direction does the Actuator Shaft rotate for MA-305, MA-405, MA6-305, MA6-405 actuators when powered up.?

Issue:
What direction does the Actuator Shaft rotate for MA-305, MA-405, MA6-305, MA6-405 actuators?

Product Line: 
Valves and Actuators 

Environment:
Product Features

Cause:
Installation / Maintenance

Resolution:
The shaft rotation of a MA-305 Actuator is Clockwise (CW) 180° when power is applied. This rotation direction also applies to MA-405, MA6-305, MA6-405 actuators.
 
Was this helpful?
What can we do to improve the information ?