Technical FAQs

Ask a Question

Are the Tesys K contactors suitable for applications in AC4 usage above 440V?

Issue:
Customer is looking to use the LC2K contactors in AC4 category. 

Product line:
LC1K, LC2K, Tesys K K-Line

Environment:
n/a

Cause:
Charts available show up to 440VAC. 

Resolution:
The LC1K series is only suitable up to a maximum of 440VAC in category AC4.  Suggest to review the LC1D, Tesys D Line contactors which have charts available in AC4 up to 690VAC. 

 

Was this helpful?
What can we do to improve the information ?