Technical FAQs

Ask a Question

Can a VT2211G13A020 be mounted vertically?

Issue:
What is the prescribed Mounting position for Erie VT/VS Two Position Spring Return PopTop Series Valves?

Product Line: 
HVAC / Field Devices

Environment:
Valves and Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
Yes, The valves can be mounted in horizontal or in a deflected vertical piping direction. When installed in horizontal direction piping, the actuator must be above the valve body, but can be installed vertically
 tilted left or right not below 85° from vertical, see diagram below.



N O T E
• Make certain there is no overhead water source that may drip onto valve actuator.
• In normal service, some condensation may occur on or around the valve. A drip pan may
be necessary or the valve body may be insulated.
Was this helpful?
What can we do to improve the information ?