Technical FAQs

Ask a Question

What is the NEMA rating of the 0453L0077GA00 damper actuator?

Issue:
NEMA rating for ALL 453X Series damper actuators?

Product Line: 
HVAC / Field Devices

Environment:
Damper Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
The enclosure is rated NEMA 1 indoor 
Was this helpful?
What can we do to improve the information ?