Technical FAQs

Ask a Question

Can a VB-7223 Series valve be converted to a 3-Way valve?

Product Line: 
HVAC / Field Devices

Environment:
Valves

Cause:
Replacement / Installation / Maintenance

Resolution:
No, removing the lower thread cap of a VB-7223 (2 -way) will not convert the valve  into a (3-way) valve. There is no internal and lower port to make it into a 3-way valve. The lower cap is only an access point to replace the stem & plug assembly. 


Was this helpful?
What can we do to improve the information ?