Technical FAQs

Ask a Question

What is the part number and watt rating of the heating element used on ATV660 units rated for 200 HP at 460V.

Issue:
What is the part number and watt rating of the heating element used on ATV660 units rated for 200 HP at 460V.

Product Line:
ATV630/660

Environment:
All

Cause:
N/A

Resolution:
The heater is a 100W, 110-250V, part # NSYCR100WU2C.
Was this helpful?
What can we do to improve the information ?