Technical FAQs

Ask a Question

Can a VT2417G13B01A valve have an end switch added for 110 V ?

Issue:
The VT2417G13B01A valve assembly has a Terminal block, and End switch, can it be ordered with 110V ?

Product Line:
Valve and Actuatora

Environment:
Application

Cause:
Product features

Resolution:

The VT2417G13B01A has a terminal block and end switch rated for only 24 VAC . For 110V switch a VT2417G13B02A Zone valve needs to be ordered. It comes with 18" leads and 110V End switch .
Was this helpful?
What can we do to improve the information ?