Technical FAQs

Ask a Question

What is the difference between ATV212WD11N4 and ATV212HD11N4?

Issue : 
What is the difference between ATV212WD11N4 and ATV212HD11N4?

Product Line :
Altivar 212

Cause :
Crossing the ATV212WD11N4 

Resolution : 
WD is a NEMA 12 version of the HD which is a NEMA 1.
Functionality, the same.
Dimensions has differences. See pictures.
Was this helpful?
What can we do to improve the information ?