Technical FAQs

Ask a Question

What determines which combinations are listed on the Quick Start Annex SCCR?

Issue:
What determines which combinations are listed on the Quick Start Annex SCCR?  

Product Line:
ATV ATS Altistart Altivar

Environment:
All

Cause:
Wiring

Resolution:
Explained that the listed combinations were tested for the 100 kA rating typically requested by customers and OEMs.  Other combinations might work as well but we can't recommend and customer's have to do the testing for that.

 
Was this helpful?
What can we do to improve the information ?