Technical FAQs

Ask a Question

Can you order the ATS22 soft starter with a specific firmware version?

Issue:
Can  you order the ATS22 soft starter with a specific firmware version?

Product Line:
ATS22 

Environment:
All 

Cause:
Wants a specific firmware version. 

Resolution:
The firmware update is done on the mfg side not the end customer side. In most cases the end customer will not need to update the firmware because their soft starter works with the previous version no problem. But if they buy a new product it will most likely include the updated firmware.
 
Was this helpful?
What can we do to improve the information ?