Technical FAQs

Ask a Question

HMIGTU dual monitor support

Issue:
Does the HMIGTU support dual monitors?

Product Line:
HMIGTU

Resolution:
The HMIG5U supports an additional monitor using the Built-in DVI port.
The HMIG3U does not have a video port so it does not support an additional monitor.



 
Was this helpful?
What can we do to improve the information ?