Technical FAQs

Ask a Question

Unity Pro force information in the PLC

Issue:
Can you see if there are forces in the PLC without using Unity Pro?

Product Line:
M340, M580, Quantum, Momentum, Premium

Environment:
Only applies to Unity Pro PLC's

Resolution:
Below are the system words that increment and decrement when forces are allied or removed. 

Word %SW108:
increments each time a discrete bit (%I,%Q, %M or DDDT) is forced.
decrements each time a discrete bit is unforced.

Word %SW109:
increment each time an analog channel is forced.
decrement each time an analog channel is unforced.
NOTE: For Quantum platform, limited to analog channels of Modicon M340 Analog Modules in remote I/O drops
 
Was this helpful?
What can we do to improve the information ?