Technical FAQs

Ask a Question

Does the Unity Momentum support located memory offset

Issue:
My Momentum addresses are offset when reading from my HMI. Is there a setting in Unity to offset the base address?

Product Line:
Momentum, Unity Pro

Environment:
171CBU78090, 171CBU98090, 171CBU98091

Resolution:
The Unity Momentum does not support base memory offset like the M340 and M580 do. See system words %SW138 to %SW141 in Unity Pro help.

 
Was this helpful?
What can we do to improve the information ?