Technical FAQs

Ask a Question

What is the correct wiring and markings on the RE88867105 timer?

 Issue:
The catalog and RE88876105 timer wiring information do not match, what is the correct wiring?

Product line:
RE8 timers

Environment:
n/a

Cause:
Catalog was incorrect

Resolution:
See the attached corrected wiring information for this timer.

 
Was this helpful?
What can we do to improve the information ?