Technical FAQs

Ask a Question

What is the maximum Frequency that can be used on the Zelio Logic relays?

 Issue:
Customer is asking for the highest frequency that can be used on the SR3B261FU Zelio Logic relays.

Product line:
Zeliologic Smart relays

Environment:
n/a

Cause:
Application

Resolution:
The maximum allowable frequency on the SR2/SR3 Smart relays is 7.37MHz

 
Was this helpful?
What can we do to improve the information ?