Technical FAQs

Ask a Question

Can I lock a base popup to call a secondary popup in Vijeo Designer V6.2?

Yes.  This allows the secondary popup to the front of the main popup.
To lock the base panel, change  Lock Out Base Panel disabled to enabled.
User-added image

Then the panel will be to the front.
   
 


Best Regards 
Schneider Electric 
Donald Dube 
888-266-8705 
customer.services@schneider-electric.com 
http://eclipse.modicon.com
 
Was this helpful?
What can we do to improve the information ?