Technical FAQs

Ask a Question

Is the Aux connector included with the HMIG5U

Issue:
Does the HMIG5U include the aux connector.

Product Line:
HMIG5U

Resolution:
The Aux connector is not included with the HMIG5U.
The part number to order it is HMIZGAUX(Pkg of 5)
 
Was this helpful?
What can we do to improve the information ?