Technical FAQs

Ask a Question

Can the VB-804 Series valves are able to use the DuraDrive and Forta Actuators?

Issue:
Compatibility of current DuraDrive and Forta actuators to old VB-804 Series Valves

Product Line: 
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement 

Resolution:
The DuraDrive and Forta actuators cannot be used with the obsoleted VB-804 Series valves. The VB-804 Series valve needs to be replaced with the updated VB-9313 Series Valves,
in order to use our current DuraDrive and Forta actuators .
Was this helpful?
What can we do to improve the information ?