Technical FAQs

Ask a Question

What is the voltage range on the ATV960 enclosed drives?

Issue:
What is the voltage range on the ATV960 enclosed drives?

Product Line:
ATV960 enclosed drives. 

Environment:
All 

Cause:
Wants to know if you can run a 208vac motor on the ATV960 enclosed 230vac rated drive.

Resolution:

The  ATV960 installation manual says the input voltage range is min 208VAC to  max 460vac .

This should cover the 208v, 230v and 240v range on the ATV960 drive 230 volt rated drive.
This should cover the 460v  range on the ATV960 drive 460 volt rated drive. 
 
Was this helpful?
What can we do to improve the information ?