Technical FAQs

Ask a Question

What is the valve part number for a Normally closed version of a VB-7213-0-4-04 valve, which is Normally open ?

Issue:
Is there a VB-7XXX series valve that is normally closed 

Product Line:
Valves and Actuators

Environment:
VB-7XXX Valve

Cause:
Application

Resolution:
A VB-7223-0-4-04 valve is for stem up normally closed operation . See Truth table below for part number variances associated with the VB-7XXX and VB-9XXX Series Valves:



 
Was this helpful?
What can we do to improve the information ?