Technical FAQs

Ask a Question

Does a VC-9323-401-5-14 assembly have a replacement?

Issue:
What valves are manufactured by Warren Controls?

Product Line: 
HVAC / Field Devices

Environment:
Valves and Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
If the customer wants a direct replacement they need to contact Warren Controls for the valve body which is the "VB-9323-0-5-14" , we don't manufacture this valve anymore. 
Having the "VB-9323-0-5-14" Valve Body, they can use the MC-351 actuator and AV-352 linkage .

If the customer option to use the crossed valve body part# "VB-8303-0-5-14"  then they will have a different actuator and linkage kit.
The customer has to provide the specification for the actuator to proceed on part selection.

Warren Controls manufacture the following valves:

VB-9323-0-5-12
VB-9323-0-5-13
VB-9323-0-5-14
VB-9323-0-5-15
VB-9323-0-5-16

Warren Controls
Phone: 800-922-0085
www.warrencontrols.com



 
Was this helpful?
What can we do to improve the information ?