Technical FAQs

Ask a Question

What is the SCCR rating for DTU switches, 240 or 600V, 600A?

Issue:
What is the Short Circuit Current Rating of a DTU326 or DTU366 Double Throw Switch?

Product Line:
Double Throw Safety Switches

Environment:
Non Fused DTU safety switches also including DTU326R, DTU426, DTU426R, DTU366R and DTU466R, series A

Resolution:
When protected by class H or J it is rated at 10Kaic and when protected by class R, J or T switch is rated at 100Kaic
 
Was this helpful?
What can we do to improve the information ?