Technical FAQs

Ask a Question

What does always mean in the R/W table of the communications manual on the ATV630 drive?

Issue:
What does always mean in the R/W table of the communications manual on the ATV630 and ATV930 drives?

Product Line:
ATV630 and ATV930 drives?

Environment:
All

Cause:
reading and writing data over the network

Resolution:
Always means you can read or write data when the drive is stopped or when its running.
 
Was this helpful?
What can we do to improve the information ?