Technical FAQs

Ask a Question

What type of connector is included with the XVGU3SWV?

 Issue:
What type of connector is included with the XVGU3SWV? 

Product line:
XVG Tower lights

Environment:
n/a

Cause:
Misprinted information in an older document shows Micro A USB connector.

Resolution:
The correct connector is a Micro B USB.  See the attached instruction bulletin

 
Was this helpful?
What can we do to improve the information ?