Technical FAQs

Ask a Question

What is the difference between an MA-418-101 and an MA-418?

Issue:
is a MA-418 Actuator the same as a MA-418-101 Actuator ?

Product Line: 
HVAC / Field Devices

Environment:
Application

Cause:
Product Features 

Resolution:
The MA-418-101 Actuator has a 90 degree rotation, while the MA-418 Actuator has a 180 degree rotation.
Was this helpful?
What can we do to improve the information ?