Technical FAQs

Ask a Question

Is there a service wrench for an MF51-7103-101?

Issue:
What is the 1-5/8" service wrench for an MF51-7103

Product Line: 
HVAC / Field Devices

Environment:
Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
The service wrench for a MF51-7103-101 Actuator is part number KEL-M-370 which is a 1-5/8" .
Was this helpful?
What can we do to improve the information ?