Technical FAQs

Ask a Question

Are Nema4X Fibeglass enclosures for our NQ, NF panels lockable?

Issue:
Do the Fiberglass N4X panel enclosures have a lock?

Product Line:
Panelboards

Environment:
N4X NQ and NF panelboards

Resolution:
No. The fiberglass enclosure handles are not lockable. The small enclosures, 26", 32" and 38" high enclosures do have provisions for providing a padlock. All other enclosures will require a third party to contact the enclosure manufacturer for locking options. Schneider/Square D does not offer anything. The enclosure manufacturer is Vynckier.
Was this helpful?
What can we do to improve the information ?