Technical FAQs

Ask a Question

What size din rail does GS1DU3 disconnect switch mount on?

Issue:
 What size din rail does GS1DU3 disconnect switch mount on?

Product Line:
UL98 IEC Style Disconnect Switches

Environment:
Accessories, LK4 Nonfusible and GS2 Fusible

Resolution:
Mounts to 35mm DIN rail (either 7.5mm or 15mm height) or directly to the panel with screws.

Note:
Mounting to 7.5mm high rail might be difficult if the rail is securely mounted to the panel, 15mm high rail will solve this problem. This is due to the bottom width of the switch.
 
Was this helpful?
What can we do to improve the information ?