Technical FAQs

Ask a Question

How many auxiliary contact can be added to VCCF02?

Issue:
What is the maximum number of auxiliary contact can be added to VCCF02?

Product Line:
Mini-Vario and Vario™ Assembled and Enclosed Switches

Environment:
UL508 Motor Disconnect Switches

Resolution:
Can add a maximum of 2 on each side.
Was this helpful?
What can we do to improve the information ?