Technical FAQs

Ask a Question

Should I use one BTS for my system or multiple BTS?

Issue:
In a system with multiple charger controllers or inverters, do I need to use a Battery Temperature Sensor in all of them or just one?

Product Line:
MPPT60, MPPT80, XW+, CSW, Battery Monitor

Environment:
Any installation including more than one inverter/charger or charge controller.

Resolution:
For best results, use multiple Battery Temperature Sensors

Cause:
Xanbus devices only use shared BTS information for emergency shutdown situation.  Charging compensation is still done according to the local BTS or the default temperature setting.
Was this helpful?
What can we do to improve the information ?