Technical FAQs

Ask a Question

Are the GS2 switches suitable for use with Corner Grounded Delta System?

 Issue:
Customer wants to use the GS2MU3N on a corner grounded Delta wiring system.

Product line:
GS2 switches

Environment:
all

Cause:
documentation does not specify.

Resolution:
The GS2 are rated for a full 480V or 600V system.  There are no restrictions with using on a Corner Ground Delta system.

 
Was this helpful?
What can we do to improve the information ?