Technical FAQs

Ask a Question

Is the VT2425G13B020 zone valve available?

Issue:
Is the VT2425G13B020 zone valve with Metric threadsa still available ?

Product Line:
Valves and Actuators 

Environment:
Maintenance 

Cause:
Replacement 

Resolution:
The 5.0CV rating for the 1" VT2425G13B020 valve, is no longer available. The higher CV (8.0), for 1" zone valve, is available as part number VT2427G13B020
Was this helpful?
What can we do to improve the information ?