Technical FAQs

Ask a Question

What replaces the VB-9315-0-4-8 valve?

Issue:
Is the VB-9315-0-4-8 valve body still available and with metric threads?

Product Line:
Valve and Actuators 

Environment:
Maintenance 

Cause:
Replacement 

Resolution:
The VB-9315-0-4-8   obsolete and it's replacement crosses to VB-7315-0-4-08. Unfortunately the VB-7315-0-4-08 valve ,with metric threads , is also no longer available.
The VB-7313-0-4-08 valve is the functional equal , but with NPT Threads and is the current offering 
Was this helpful?
What can we do to improve the information ?