Technical FAQs

Ask a Question

Will the GS2 or LK4 accessories work with the 9421 or 9422 disconnects?

 Issue:
Customer has the 9421LJ4 but wants to the use the handles from the GS2 series for a smaller, round instead of the flange operated.

Product line:
9421 9422  GS2 LK4 Op Mech

Environment:
n/a

Cause:
n/a

Resolution:
No, the GS2 and LK4 accessories including the handles, shafts, auxiliary contacts will not work with the NEMA 9421, or NEMA 9422 series disconnect switches or Operating Mechanisms.

 
Was this helpful?
What can we do to improve the information ?