Technical FAQs

Ask a Question

Is separate control power needed for the ATS22-S6U models?

 Issue:
Do they need separate control power or does the line voltage power the display on the ATS22-S6U?

Product line:
Altistart 22, ATS22

Environment:
S6U models

Cause:
n/a

Resolution:
The models ending in S6U use a separate 120VAC power source to power up the display and the logic inputs. 

 
Was this helpful?
What can we do to improve the information ?