Technical FAQs

Ask a Question

What is the altitude de-rating for the GV7R Manual Motor Controllers?

 Issue:
Customer wants to use the GV7RE100 at 4600m

Product line:
GV7 Manual Motor Controllers

Environment:
Altitude

Cause:
Derating is not shown in the documentation.

Resolution:
The derating factors to be applied for main pole operational voltage and current of GV7R are as follows:
 
Altitude (m)                                                          2000                      3000                     4000                     5000
Rated operational voltage (V) Ue                            690                        550                       480                       420
Average thermal current (A) at 40 °C                      1xIn                       0.96xIn                 0.93xIn                 0.9xIn
 

 
Was this helpful?
What can we do to improve the information ?