Technical FAQs

Ask a Question

Can you use 110Vac on CL1, CL2 and another separate 110Vac for the start command on an ATS22..S6U?

Issue:
Can you use 110Vac on CL1, CL2 and another separate 110Vac for the start command on an ATS22..S6U?

Product Line:
Altistart ATS22
 
Environment:
All

 
Cause:
Wiring

 
Resolution:
ATS22...S6U requires Control Power supply 110Vac -15 % 115Vac +10% 

Close 110Vac to CL1, and neutral to CL2 from your Control Power.  You can use the same or a separate 110Vac to close to LI1, LI2 for the run command from your contactor.
Was this helpful?
What can we do to improve the information ?