Technical FAQs

Ask a Question

How does a VT2212 differ from a VS2212?

Issue:
How does a VT zone valve differ from a VS zone valve?

Product Line: 
HVAC / Field devices

Environment:
Valves and Actuator

Cause:
Installation/Set-up/Application Assistance

Resolution:
The difference between a VT from a VS zone valve is the temperature rating. A Zone valve part number starting with "VT" , is rated for general temperature usage and NOT for use with Steam.
On the other hand, the Zone valve starting with "VS", IS rated for Steam and a higher temperature.

See table below for temperature range.



 
Was this helpful?
What can we do to improve the information ?